3/18/2021 10:09 AM | |
Posts: 2 Rating: (0) |
Hello After wrong done battery replacement I have been asked to load parameters to machine Burkhardt Weber MC60 from 1992. I figured out that also PLC was erased. I performed overall reset +cold restart. Now PLC won start. From checked ISTACK and BSTACK. In Stop Cause signed are : STP and UPROG. in Depth 1 only one stop cause is signed : SUF. Could you advice me how to diagnose this issue? s5d file of plc afer reset attached. Attachmentplc2021.zip (458 Downloads) |
3/18/2021 10:38 AM | |
Posts: 2 Rating: (0) |
attached ISTACK and BSTACK OK. after some night readig of internet and manuals I figured out that my problem is command: This command gives me a Substitution error (SUF ) and STOP the PLC because I don't have OB27 in EPROM OB27 should handle this error. AttachmentIstack+Bstack.zip (511 Downloads) |
Last edited by: Flower1710 at: 03/19/2021 11:42:51Last edited by: Flower1710 at: 03/21/2021 21:40:18 |
|
6/19/2023 12:50 PM | |
Joined: 6/19/2023 Last visit: 6/21/2023 Posts: 2 Rating: (0) |
we use same machine. Can you send me your contact for some consultations please. |
6/21/2023 8:03 AM | |
Joined: 6/19/2023 Last visit: 6/21/2023 Posts: 2 Rating: (0) |
can you send me his email? |
6/21/2023 11:35 AM | |
Joined: 8/3/2017 Last visit: 5/3/2024 Posts: 1085 Rating: (53) |
Hello AutoGen, I'm just a normal user, just like you.. and thanks to the data protection regulations, no personal data is shared and sharing of such data is forbidden according the forum rules, so: no Contact Siemens directly via a SR or start your own topic. |
Please, check out the forum search to find already existing topics regarding your issue and to get some hints. |
|
Follow us on