5/17/2023 9:07 AM | |
Joined: 7/19/2022 Last visit: 5/22/2024 Posts: 358 Rating: (61) |
Hello MPBusuttil, The maximum memory size is allocated when you create the data log. Besides ensuring enough memory space for all the data records, you must take into account the memory space of the following elements for the memory allocation:
The formula below represents a method to help you determine the estimated size of your data log. Make sure that you observe the rule for the maximum size. Data bytes of the data log = ((data bytes in a data record + time stampbytes + 12 bytes) * number of data records) |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to2 thankful Users |
5/17/2023 9:39 AM | |
Joined: 3/11/2019 Last visit: 5/23/2024 Posts: 1430 Rating: (259) |
Hi, Information to the formula above and also an example can be found here. Limit to the size of data log files
regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
Follow us on