9/1/2021 8:19 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Hello, P042 is parameter to display frequency. You can connect the source connector of which frequency you want to display. p421 is function parameter to set upper limit of motorised potentiometer value. Please check which values are displayed in it & compare with your drive logic. For more details, please refer SIMOVERT MASTERDRIVES, VECTOR CONTROL, COMPENDIUM manual. HTH |
Follow us on