11/17/2022 8:15 AM | |
Joined: 5/12/2006 Last visit: 6/10/2024 Posts: 22258 Rating: (2987)
|
where is the dcc chart in the project? CPU or DRIVE? |
11/18/2022 4:41 AM | |
Joined: 5/12/2006 Last visit: 6/10/2024 Posts: 22258 Rating: (2987)
|
the drive can not be simulated, so also the dcc charts can't be simulated |
11/18/2022 9:07 AM | |
Joined: 5/12/2006 Last visit: 6/10/2024 Posts: 22258 Rating: (2987)
|
download it to simosim |
11/21/2022 2:30 AM | |
Joined: 1/17/2013 Last visit: 5/27/2024 Posts: 1087 Rating: (6) |
Dear ChristophD, I will try Thank you. |
Best Regards, |
|
11/22/2022 9:05 AM | |
Joined: 5/12/2006 Last visit: 6/10/2024 Posts: 22258 Rating: (2987)
|
check if CFC is installed and have a valid Licence |
Follow us on