5/16/2024 3:06 PM | |
Joined: 2/3/2023 Last visit: 5/29/2024 Posts: 4 Rating: (0) |
In which software was the bug located? In a piece of javascript you created or in the Siemens firmware? |
5/17/2024 6:44 AM | |
Joined: 5/8/2012 Last visit: 6/11/2024 Posts: 32 Rating: (3) |
I have the same problem when I try to do delta download into remote OS. I tried to delete IM folder of my project (https://support.industry.siemens.com/cs/document/109778709/how-do-i-delete-the-im-folder-of-my-tia-portal-project-?dti=0&lc=en-IT) - no result. When I start RT as "simulation" and try to do delta download - all is ok. The problem is only when I try to do delta download into remote OS. |
Last edited by: last_bu at: 05/17/2024 06:45:02Last edited by: last_bu at: 05/17/2024 07:00:06Last edited by: last_bu at: 05/17/2024 07:02:34Last edited by: last_bu at: 05/17/2024 07:09:38Last edited by: last_bu at: 05/17/2024 07:19:00 |
|
5/17/2024 7:12 AM | |
Joined: 1/21/2013 Last visit: 6/12/2024 Posts: 2882 Rating: (460)
|
Hi last_bu, Since you are comparing with the simulation, I assume that you are working with a Unified Comfort Panel. In this case, a possible reason why a delta download cannot be started is that the Runtime startup process could not be completed. If the Runtime is not fully started, it may not allow a delta transfer. However, to find out the reason for this, you need to at least get some trace data from your device and look for the reason there. But to be honest, this is something that should be done by Siemens. So you should report your problem to technical support. Kind regards |
5/17/2024 7:22 AM | |
Joined: 5/8/2012 Last visit: 6/11/2024 Posts: 32 Rating: (3) |
No, I am working with PC. And I try to do delta download only when startup process is completed.
|
Last edited by: last_bu at: 05/17/2024 07:24:50 |
|
5/17/2024 8:02 AM | |
Joined: 5/8/2012 Last visit: 6/11/2024 Posts: 32 Rating: (3) |
Thank you Stefan!
|
Follow us on