2/5/2024 1:07 PM | |
Joined: 11/22/2023 Last visit: 3/18/2024 Posts: 5 Rating: (0) |
Hello Stefan, SQLLAKLIJNDEVION is the instance name of my SQL server. Normally when connecting to an SQL server you can connect with IP-adres and port or you can connect directly to the SQL instance defined by the IP-adres or the PC name /Instancename. I tried it without it with the following connection string: But it didn't work, I get the following error: I used 127.0.0.1 since I'm testing the connection first via browser on the device where my SQL server is located. Best regards, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/16/2024 06:40:08New subject after splitting |
|
Follow us on