6/28/2023 12:57 PM | |
Joined: 6/28/2023 Last visit: 6/28/2023 Posts: 1 Rating: (0) |
Hello Everyone, I have 6ES7148-4FC00-0AB0 module. on which I'm planning to connect one light curtain and one E-stop. light curtain will get supply from VS1 and ) vdc from the 6ES7148-4FC00-0AB0 module port and simply give OSSD1 and OSSD2 signal to the F module. on second port vs1 and vs2 will be passed through the estop 2 NC contacts and returning to F module as safe signals. but problem I'm getting is when I try to enable short circuit detection function through software my F module goes in error mode. I think this is because I'm getting only ossd signals from light curtain and I don't require short circuit or cross connection monitoring for light curtain. please do let me know if anyone has solution over it. Thanks in advance, Sharad ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/29/2023 07:23:33New subject after splitting |
|
6/30/2023 2:36 PM | |
Joined: 8/6/2018 Last visit: 6/12/2024 Posts: 251 Rating: (39) |
Hello, Could you send us a wiring diagram? Thanks you |
Follow us on