11/14/2022 10:48 PM | |
Joined: 9/27/2006 Last visit: 6/7/2024 Posts: 12260 Rating: (2670)
|
Hello Lieven Borms; The S7-313c comes in 3 format designs, one is a S7-313C-2DP which can be used as a node (master or slave) on a Profibus network. See the attachment below. Siemens has created special technological functions exclusive to the S7-313C and S7-314C CPUs. Look up the manual here, and select the function you want to implement (such as Positioning with digital outputs) and follow the wiring and programing guidelines in the manual. And take into account the addresses of the integrated I/O of the S7-313C-2DP, which are different than the ones reserved for the S7-314 IFM. https://support.industry.siemens.com/cs/ca/en/view/12429336 Hope this helps, |
Last edited by: dchartier at: 11/14/2022 23:07:59Last edited by: dchartier at: 11/14/2022 23:51:44 |
|
This contribution was helpful to1 thankful Users |
11/15/2022 7:49 AM | |
Joined: 6/19/2017 Last visit: 6/10/2024 Posts: 8147 Rating: (165) |
New question published by Lieven Borms is split to a separate thread with the subject 314IFM migration from Step 7 to TIA - replace block. Best regards |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
Follow us on