4/30/2024 6:37 PM | |
Joined: 1/9/2024 Last visit: 5/4/2024 Posts: 4 Rating: (0) |
HI I have a problem with saving the STRING and DTL variable in TIA Portal to an MS SQL table. I have columns there (INT, NVCHAR, DataTime) in SQL and the data cannot be saved. When I only have one or a few VARIABLES (INT) , everything is fine and the data is written to SQL. Please help. MG ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/02/2024 08:18:54New subject after splitting |
|
4/30/2024 6:52 PM | |
Joined: 12/18/2014 Last visit: 5/17/2024 Posts: 33047 Rating: (4082) |
Please don't post twice for the same problem. Yo made also a own topic: Data Save to MS SQL Problem VB Script |
This contribution was helpful to1 thankful Users |
5/2/2024 8:20 AM | |
Joined: 6/19/2017 Last visit: 5/17/2024 Posts: 8045 Rating: (164) |
Closed cause question posted twice. The second thread with the subject Data Save to MS SQL Problem VB Script is published within the conference SIMATIC WinCC (TIA Portal). Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on