4/26/2016 5:15 PM | |
Joined: 3/17/2013 Last visit: 6/9/2024 Posts: 481 Rating: (43) |
Hi HDD and CDD represent the number of degrees over a period in which the ambient temperature is lower or higher than a base level In some of the published papers it is mentioned that , It is used both statistically in thermal load calculations and to maintain interior dwelling temperature Nothing authentically linear variations still. See one of the papers here http://www.pacificeconomicsgroup.com/jad/Mid%20Range.pdf Vijay |
This contribution was helpful to1 thankful Users |
4/29/2016 8:23 PM | |
Posts: 198 Rating: (36) |
if we will ignore this degree of day so what is disadvantage. how it will effect our buildings ?
|
Follow us on