10/6/2022 11:10 AM | |
Joined: 4/28/2015 Last visit: 5/21/2024 Posts: 9 Rating: (1) |
Hello gera98eleven, this is a known issue, that came in several times within the last weeks. Development already fixed it, probably with the next version of Flow Creator it will be included. Unfortunately there is no relyable workaround for that. If the Flow Creator hung up in loading page, you can try to simply close the tab and reopen the Flow Creator UI - but that workes only sometimes. |
10/6/2022 3:55 PM | |
Joined: 5/20/2021 Last visit: 3/19/2024 Posts: 7 Rating: (0) |
Hello. Yes, I have tried cleaning browser, cache, cookies, etc. and retry to open. But the problem remains, the only solutions I have found is uninstalling the Flow Creator, but immediately I close the tab, doesn't matter if I logout or not, when I try to open the app get stuck again. My IED version: 1.5.0.5-e IED Flow Creator v1.3.9 Logs of IE Flow Creator it´s on the attachment. I don't look errors in the log, maybe this is a version bug or something like that. I'll very grateful if you can help me. Thanks. AttachmentFlow Creator log.zip (666 Downloads) |
Follow us on