3/4/2024 10:06 AM | |
Joined: 8/29/2019 Last visit: 4/30/2024 Posts: 4 Rating: (1) |
Hello, i have also same issue. i have TIA v18 update 1 and SIMATIC_WinCC_Legacy_Panel_Images_V18 installed in laptop. TP700 comfort firmware version is v17.0.0.5. TP700 restart while downloading the project into device and got error Adaptation of target device failed. if anyone have solution please replay. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 03/05/2024 10:06:04New subject after splitting |
|
3/27/2024 9:28 AM | |
Joined: 8/3/2009 Last visit: 5/16/2024 Posts: 12951 Rating: (1650)
|
Hello ket2 I think there should be an Upd6 Image available but you should be able to download also without doing the OS update. If you have problems you can also try to do a offline Transfer: https://support.industry.siemens.com/cs/de/en/view/109740696 Bye Murof |
If this Information really helps, you could use the Rate function |
|