4/23/2024 5:37 AM | |
Joined: 1/21/2013 Last visit: 5/20/2024 Posts: 2798 Rating: (452) |
Hi alpaslane, It's ok and recommended to use the X1 interface for a S7-1500 Software Controller with version 30.0 or newer. This is because version 30.0 removes the PC station and therefore it is not possible to load the complete device on the first download. The text in the manuals has been changed accordingly. I was not aware of the changes because my last download to an Open Controller was with V17 and therefore with a version older than 30.0. Kind regards |
This contribution was helpful to1 thankful Users |