3/13/2024 6:35 PM | |
Joined: 10/7/2020 Last visit: 4/27/2024 Posts: 21 Rating: (0) |
Hello all, I am using TIA Portal v17 update 1. I have a redundant PLC, 1513R-1 PN (6ES7 513-1RM03-0AB0). But I have configured the PLC as 6ES7 513-1RL00-0AB0 on TIA Porta (I asked about this when I bought the PLCs and it works properly) This is the tird project with the same layout, there are just small changes between the projects. The problem started when the KTM700s (three of them) did not communicate with this redundant PLC but they did with the others PLCs. At that moment I decided to break the HMI connections, create them again, compile all and download to the devices. When I tried to download to the PLC I got this alarm:
The project is installed on a vessel the leaves next week so I am in a hurry. Everything works but this communication and the download to the redundant PLC. Can someone guide me? Thank you in advance, Gorka I am attaching the document with the logs AttachmentError downloading program to PLC - log.pdf (21 Downloads) |
3/14/2024 7:03 AM | |
Joined: 10/7/2020 Last visit: 4/27/2024 Posts: 21 Rating: (0) |
Hi 0_Einstein, I have tryed to update the firmware to 2.9 but I cannot download it to the PLC. In any case, where can I check this error code? I checked here: https://support.industry.siemens.com/cs/it/en/view/109766300 But I did not find any error code. Is there a site or software where I can check the error code? Thank you for your help, Gorka |
Last edited by: The Helping Hand at: 03/14/2024 12:17:29Link optimized |
|
3/14/2024 4:12 PM | |
Joined: 7/7/2010 Last visit: 5/10/2024 Posts: 14709 Rating: (2359) |
You already had the answer.
|
science guy |
|