4/15/2024 3:23 AM | |
Joined: 12/18/2014 Last visit: 5/17/2024 Posts: 33051 Rating: (4082)
|
Import of a technical question via PM from the user AutoGen_1556928 ---------------------------------------------- This is an English speaking forum.
Translate to English:
|
This contribution was helpful to1 thankful Users |
4/15/2024 3:26 AM | |
Joined: 12/18/2014 Last visit: 5/17/2024 Posts: 33051 Rating: (4082)
|
We need more details. How should the burner be controlled? Just switch it on and off via a digital output? |
4/15/2024 4:50 AM | |
Joined: 2/18/2024 Last visit: 5/8/2024 Posts: 16 Rating: (0) |
Le contrôle du brûleur se fait par un simple contact câblé sur une sortie du logo |
4/15/2024 6:44 AM | |
Joined: 2/18/2024 Last visit: 5/8/2024 Posts: 16 Rating: (0) |
The burner is controlled by a simple wired contact on a logo output |
4/15/2024 6:55 AM | |
Joined: 12/18/2014 Last visit: 5/17/2024 Posts: 33051 Rating: (4082)
|
Try this ...
AttachmentBurner_0BA8.Standard.zip (12 Downloads) |
4/15/2024 7:02 AM | |
Joined: 2/18/2024 Last visit: 5/8/2024 Posts: 16 Rating: (0) |
THANKS. I will test the program and I will tell you the result. Is it necessary to calibrate the pt100?
|
4/15/2024 9:43 AM | |
Joined: 12/18/2014 Last visit: 5/17/2024 Posts: 33051 Rating: (4082)
|
That may be possible. It depends on which PT you have (2-, 3- or 4-wire) and the cable length and cross-section. |
4/18/2024 8:59 AM | |
Joined: 12/18/2014 Last visit: 5/17/2024 Posts: 33051 Rating: (4082)
|
English please ... I don't speak French. |