11/29/2005 12:48 PM | |
Joined: 8/31/2005 Last visit: 5/16/2024 Posts: 217 Rating: (40) |
Hi cream! The SFC 82 can not be used in an S7-400 PLC (For available SFCs in an S7-400 PLC check the instruction list: http://support.automation.siemens.com/WW/view/en/1117645, chapter "System Functions", p. 106). This is because the SFC 82 is only for use with MMC (Micro Memory Card) and these MMCs are only used in S7-300 PLCs or ET 200S. |
Last edited by: Chris at: 11/29/2005 12:50 PMGreetings, Chris |
|
Follow us on