3/30/2024 11:46 AM | |
Joined: 3/13/2019 Last visit: 5/7/2024 Posts: 149 Rating: (2) |
Dear sir, Pls help on this ,I am still waiting for reply... Regards, Pankaj Tiwari |
3/31/2024 1:18 PM | |
Joined: 2/28/2023 Last visit: 5/7/2024 Posts: 36 Rating: (1) |
Hi Pankaj Accordingly, the hardware configured for the MicroMaster 440 is in a reverse mode with command source P0700 enable at terminal 6 (digital input 2) with supply of 24voltage. To activate the default P0700 command source P0700 should be set to 12 (ie P0702-12) otherwise 2 (ie P0702-2). Please for further information MM440_OPI_English.pdf (siemens.com) ------------------------------------------------------------------------------------------------------ Is it resourceful? Rate it if you wish not an obligation |
Cheers. |
|
Follow us on