11/11/2022 10:46 AM | |
Joined: 11/10/2022 Last visit: 2/27/2023 Posts: 10 Rating: (0) |
Thanks for your answer. Did I understand correct servo using passive encoder for servo control? |
11/11/2022 10:51 AM | |
Joined: 11/10/2022 Last visit: 2/27/2023 Posts: 10 Rating: (0) |
I have few faults from C1 axis drive system sinumerik 810D |
11/18/2022 6:54 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873)
|
Please set parameter values as below & check. MD30200 = 1 Retain MD30240[0] &[1] values as per original. |
2/11/2024 12:05 PM | |
Joined: 5/18/2015 Last visit: 5/8/2024 Posts: 98 Rating: (1) |
Hello I have SINUMERIK 840D and one external encoder on spindle Gear box If i discount encoder socket on X421 , show Alarm 25000 and 25001 If connect socket on X421 , have only 25001 alarm. If change MD30200 from 2 to 1 or 0 , after push machine on button, communication nc fail and MD30200 back 2 automatic 😐. How can i use only one encoder for spindle motor? Thanks. AttachmentSINUMERIK 840D SP fault of passive encoder (2).pdf (131 Downloads) |
SKAZEMCNC |
|
Follow us on