6/11/2023 1:30 PM | |
Joined: 6/14/2015 Last visit: 4/25/2024 Posts: 236 Rating: (1) |
Hello every body. I need touch screen driver for IPC477C.where can I download it? |
6/11/2023 4:38 PM | |
Joined: 12/28/2016 Last visit: 5/9/2024 Posts: 429 Rating: (44) |
Hello The touch screen driver for IPC477C can be downloaded from the official website of Siemens. Here are the steps to download the driver: 1. Go to the Siemens Industry Online Support website (https://support.industry.siemens.com/). 2. Click on "Downloads" in the top menu bar. 3. Under "Product Support," select "Industrial Automation and Control." 4. Navigate to "Human Machine Interface (HMI)" and select "SIMATIC HMI IPC." 5. Select "IPC477C" as your device. 6. Under "Drivers," select "Operating System-independent" and then select "Touch Driver." 7. Click on "Download" to start the download process. Once the download is complete, follow the installation instructions provided with the driver to install it on your IPC477C.
|
https://pnap.ir |
|
Follow us on