1/11/2023 8:34 PM | |
Joined: 1/21/2013 Last visit: 6/4/2024 Posts: 2839 Rating: (455) |
Hi KianParax, I assume the four axes should work together in a coordinated way. To make this possible with the motion control technology objects of a S7-1500, you need to use a technology CPU. For working with G-Code maybe the SIMATIC S7-1500T Kinematics Language would be interesting to you. Since this is the design of a more complex system, I would recommend that you contact the technical consulting service. Kind regards |
1/15/2023 9:30 AM | |
Joined: 1/21/2013 Last visit: 6/4/2024 Posts: 2839 Rating: (455) |
Hi KianParax, the SIMATIC S7-1500T Kinematics Language is designed for the technology object "Kinematics". For this you need a S7-1500T. Kind regards |
This contribution was helpful to1 thankful Users |
Follow us on