11/3/2022 8:08 PM | |
Joined: 4/28/2015 Last visit: 6/7/2024 Posts: 37 Rating: (1) |
Hello, I am trying to install the Telit 5G FN980 radio. Using the proper slot x101. I don't see any text in the dmesg or lsusb does not show the Telit radio. However, if I place the same radio on a USB/M.2 Carrier and plug it into the USB port we can see the radio. "lsusb" finds it and we can see the 5 /dev/ttyUSBx ports ready and responding. How can I setup the x101 to be USB and not PCIe? Is tehre a way to boot into some BIOS? Thanks D ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/04/2022 07:48:41New subject after splitting Last edited by: Jen_Moderator at: 11/07/2022 07:23:07Headline optimized. |
|
Follow us on