5/14/2024 11:06 AM | |
Joined: 3/11/2019 Last visit: 6/10/2024 Posts: 1460 Rating: (264) |
Hi again,
TCP/IP, or Modbus TCP specifically? Because as mentioned above, this are differnet stories. You can build a TCP communication also via TCON/TSEND/TRCV, information can be found here: Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300/S7-400 CPU?regards sancruz |
Feedback appreciated, please rate |
|
Follow us on