3/25/2022 7:29 AM | |
Joined: 1/11/2019 Last visit: 4/30/2024 Posts: 702 Rating: (140)
|
Hello Zankkar, Usually in the upgradation perspective, there are two options: with or without the utilization of the functionality of the newer version (9.1 in this case). It is recommended to go through this manual perform the upgradation based on your requirement: I have linked the relevant forum query which was posted earlier. Kindly go through the same. It would defiantly help you Updating PCS7 V9.0 to V9.1 and supported windows versions And please consider the below steps/checklist while upgrading.
Hope it helps you! |
This contribution was helpful to2 thankful Users |
3/25/2022 8:52 AM | |
Joined: 2/7/2020 Last visit: 1/10/2024 Posts: 101 Rating: (0) |
Thank you for details. :)
|
4/29/2024 6:16 PM | |
Joined: 5/25/2017 Last visit: 5/1/2024 Posts: 7 Rating: (0) |
can you please tell me how did you solve this problem , i face the same issue |
4/30/2024 4:57 AM | |
Joined: 1/11/2019 Last visit: 4/30/2024 Posts: 702 Rating: (140)
|
Kindly follow the above steps |
Follow us on