3/18/2024 7:54 AM | |
Joined: 12/18/2014 Last visit: 6/9/2024 Posts: 33166 Rating: (4098)
|
Import of a technical question via PM form the userU_e9d92d85-23ef-4f4f-a8cc-7513573dedec Hello sir, Hope you are well. I am facing problem which require your expertise to assist. 1. We have a HVAC system installed with LOGO V8.1. Trying to enter the program using LSC 8.2 but password prompted. Do we need to downgrade the LSC to 8.1 in order to open program in LOGO V8.1? 2. We have a new LOGO V8.3 where we are trying to upload the program backup programmed in LOGO V8.1. Password prompted. Trying to export V8.1 program to a new program and upload to LOGO V8.3 but still password prompted. Kindly seek your help. Thanks in advance |
This contribution was helpful to1 thankful Users |
3/18/2024 7:23 PM | |
Joined: 6/11/2019 Last visit: 6/5/2024 Posts: 2201 Rating: (98) |
@ Autogen_6306791, Was a password set for the 8.1 version? Is the unencrypted source available? |
Follow us on