8/22/2006 6:54 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (316)
|
[quote user="Gromit"]1. Do I need connecting adapter (6ES7195-1BE00-0XA0)? 2. Is it possible to connect the Simocode pro (which is in the same switch box as OBT) to OBT via terminals A and B (not via 9 pin plug)? 3. Are there every thing needed in the tool set 6GK1901-0FB00-0AA0 for assembling plugs to plastic optics (6XV1821-0AH10) ? Where could I find an instruction for work with that tools set? 4. Is it possible to use the cable 6XV1821-0AH10 outdoor (protected in plastic tube from the sun and mechanical damages, but with ambient tempearture +50…-20°C? Hi Gromit, The answers on your questions are: 1. No not for the Simocode; 2. Yes, but it is for the EMC better to do it with the Profibus FC stecker; 3. No, you may need also the PROFIBUS Plastic Fiber Optic Tool Set (6GK1905-6PA10); SIMATIC NET PROFIBUS Networks 4. In the above handbook are also all specifications of the cable you mentioned, I see no problem when you do that -30…+70°C; |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on