3/19/2024 8:05 PM | |
Joined: 3/20/2019 Last visit: 4/18/2024 Posts: 3 Rating: (0) |
Has anybody ran into this situation before? " Had a F061 - Incorrect Parameterization, downloaded program back again, alarm continued, but after a while without me doing anything i was able to acknowledge fault. But when navigating through drive monitor, the fault message comes back and parameters deactivate. Will this indicate an issue with the RAM memory? If i download again, i can get the values back, but when enabling the drive for operation, this happens again. Any input is much appreciated, Let me know if you need further information. " ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/20/2024 11:04:52New subject after splitting |
|
3/22/2024 1:45 AM | |
Joined: 6/4/2008 Last visit: 5/22/2024 Posts: 1484 Rating: (322)
|
Hi, the manual is a useful document to analyse faults. The parameter r949 will indicate which parameter is at fault Regards, Graeme |
3/24/2024 7:28 AM | |
Joined: 6/14/2015 Last visit: 4/25/2024 Posts: 236 Rating: (1) |
because you download parameter whit PC,and some parameter has wrong value .please check r949 parameter .it show you which parameter is wrong value |
Follow us on