Technical Forum

SIMATIC WinCC

PLC Siemens communication help!

Thread Starter: Adriann22   Started: 4/23/2012 11:51 AM   Replies: 9

« Previous thread Next thread »
Page 1 of 1 (10 items)
  4/23/2012, 11:51 AM
Joined 4/18/2012
Last visit: 6/15/2012
Posts: 13
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
So, I have a PLC Siemens, with 314C-2DP CPU, 6ES7 314-6CF00-0AB0, firmware V1.0 . It is my final project for my faculty and, this is the configuration and I can't buy a better version, I can't upgrade it. I have to do it with what I have. 

So, the problem is that I have to find a solution to monitorize data from distance to maintain a constant level of water in a tank, and also give commands and alarms. I've read about Web2PLC function, but it's not available for this CPU. 

Can you please help me with ideas on how could I do it? I've also been thinking to monitor data values on a computer, and from another computer log in via TeamViewer and extract data and so on.

But it's the worst case solution, in case I don't find another. 

I look forward for your response.  Thank you in advance! :)



=== Edited by Adriann22 @ 4/23/2012 11:52 AM [GMT ] ===


Top
  4/23/2012, 4:39 PM
Joined 10/26/2011
Last visit: 4/17/2014
Posts: 283
Rating:
Rated: Excellent [4.57 out of 5 / rated 56 time(s)]. (56) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

one question, do you use PCS 7 or WinCC or nothing of both?

Regards

With best regards,
Thunderstorm
Top
  4/23/2012, 5:28 PM
Joined 4/18/2012
Last visit: 6/15/2012
Posts: 13
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I use Simatic Manager Step 7, and also WinCC. But mostly Step 7.
Top
  4/24/2012, 9:28 AM
Joined 12/27/2007
Last visit: 9/10/2013
Posts: 261
Rating:
Rated: Very Good [2 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
You can use the functionality of Web Navigator, where remote monitoring of data is possible.
I think this request should be transferred from PCS 7.

Regards,
Prats
Top
  4/24/2012, 9:31 AM
Joined 10/26/2011
Last visit: 4/17/2014
Posts: 283
Rating:
Rated: Excellent [4.57 out of 5 / rated 56 time(s)]. (56) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

if you want to see some data, the you have to use WinCC.
CFC Online and CFC Trend which are in the SIMATIC Manager are only for testing of the engineering.

Regards

With best regards,
Thunderstorm
Top
  4/24/2012, 8:16 PM
Joined 4/18/2012
Last visit: 6/15/2012
Posts: 13
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Prats wrote:
You can use the functionality of Web Navigator, where remote monitoring of data is possible.
I think this request should be transferred from PCS 7.


Can you tell me more please? I haven't worked with this function of WinCC yet. :)
Top
  4/24/2012, 8:25 PM
Joined 4/30/2008
Last visit: 4/17/2014
Posts: 941
Rating:
Rated: Excellent [4.02 out of 5 / rated 54 time(s)]. (54) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Web navigator is used to send your wincc pages over th eethernet as a web page so multiple computers can see them. another nice add on is datamonitor which allow you to print reports or lend data to a exellspreadsheet

Regards


Steve

I have a very responsible position here
everytime something goes wrong i'm responsible
Top
  4/24/2012, 9:54 PM
Joined 4/19/2008
Last visit: 4/1/2014
Posts: 1370
Rating:
Rated: Outstanding [3.99 out of 5 / rated 128 time(s)]. (128) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Adriann22 wrote:
Prats wrote:
You can use the functionality of Web Navigator, where remote monitoring of data is possible.
I think this request should be transferred from PCS 7.


Can you tell me more please? I haven't worked with this function of WinCC yet. :)


Hello Adriann22,

Have a look on the Application Example With Code.

Documenting Operations Using WinCC WebNavigator

But to Used this in your Project You need a License..... & as I know the Server with 3 Client will Cost to High for your Project.

You can see the Functionality what you canused have a look on the Siemens Demo

WinCC/WebNavigator and WinCC/DataMonitor demo access






Ammy

New for every one..............

“No duty is more urgent than that of returning thanks.”
If Problem Solved......!
I can't help you privately - please post in the Forums
Top
  4/27/2012, 9:37 AM
Joined 4/18/2012
Last visit: 6/15/2012
Posts: 13
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
It's a wonderful idea and thank you for it, but unfortunetly, I can't afford to buy the license. Any other ideas, preferably that are free? :)
Top
  4/27/2012, 10:27 AM
Joined 4/30/2008
Last visit: 4/17/2014
Posts: 941
Rating:
Rated: Excellent [4.02 out of 5 / rated 54 time(s)]. (54) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Try reading this link it might help you

https://www.automation.siemens.com/WW/forum/guests/PostShow.aspx?PageIndex=1&PostID=362892&Language=en#top


Regards


Steve

I have a very responsible position here
everytime something goes wrong i'm responsible
Top
Page 1 of 1 (10 items)
Actions