Technical Forum

STEP 7 / STEP 7 Lite

license key related problem

Thread Starter: montex   Started: 4/28/2009 1:36 PM   Replies: 10

« Previous thread Next thread »
12» Page 1 of 2 (11 items)
  4/28/2009, 1:36 PM
Joined 4/28/2009
Last visit: 8/3/2011
Posts: 12
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
i have installed step & v5.4 in my laptop and i have an Automation License manager v4.0 in my laptop.i have instlled license key for step 7 in laptop.my step & application is running properly without any error and it uses the license key but it is not shown in automation license manager.
Top
  4/28/2009, 3:44 PM
Joined 4/24/2006
Last visit: 4/24/2014
Posts: 5404
Rating:
Rated: Excellent [4.18 out of 5 / rated 500 time(s)]. (500) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear montex,

Looks you are not the only one:
https://www.automation.siemens.com/WW/forum/guests/PostShow.aspx?PageIndex=1&PostID=137288&Language=en#top

Do you already have Servicepack 2 of Automation License Manager v4?
http://support.automation.siemens.com/WW/view/en/114358

Best regards,

Wizard
Top
  4/29/2009, 8:59 AM
Joined 11/15/2006
Last visit: 4/24/2014
Posts: 1188
Rating:
Rated: Outstanding [4 out of 5 / rated 125 time(s)]. (125) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hey there,

Is there an error message showing somewhere at startup the the cryptographic provider initialization failed? If so, you need to delete the folder C:\Documents and Settings\All Users\Application Data\Microsoft\Crypto - but create a backup before. Then restart your system.

Have Fun!

TomDeWou
Top
Thank you for this post from:
  5/6/2009, 6:19 AM
Joined 10/13/2007
Last visit: 4/22/2014
Posts: 19
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi... I also have the same problem as montex. No there is no any error like - cryptographic provider initialization failed? My simatic manager is working properly using the license key which is not shown by ALM. (The ALM  do not show any of the license key i.e. not trial license key also, the view in ALM is completely blank)

Regards,
Niraj P
Top
  5/6/2009, 10:16 AM
Joined 1/4/2008
Last visit: 4/16/2014
Posts: 691
Rating:
Rated: Outstanding [3.4 out of 5 / rated 84 time(s)]. (84) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,
I've seen this behaviour on our customers PC. It was solved by installation of the SP2 for the ALM V4 as suggested above.

Regards
Sydney
Top
  7/31/2009, 3:59 PM
Joined 6/30/2009
Last visit: 7/31/2009
Posts: 9
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
TomDeWou wrote:

Is there an error message showing somewhere at startup the the cryptographic provider initialization failed? If so, you need to delete the folder C:\Documents and Settings\All Users\Application Data\Microsoft\Crypto - but create a backup before. Then restart your system.


I just had this problem. The solution worked. Thx!

To delete i used the cmd
del /s Crypto
rd /s Crypto

Top
Thank you for this post from:
  8/3/2009, 11:51 AM
Joined 4/22/2008
Last visit: 1/10/2012
Posts: 32
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
TomDeWou wrote:
Hey there,

Is there an error message showing somewhere at startup the the cryptographic provider initialization failed? If so, you need to delete the folder C:\Documents and Settings\All Users\Application Data\Microsoft\Crypto - but create a backup before. Then restart your system.


Thank you, this helped me alot.

Best regards
Daniel Nilsson
Top
  9/2/2009, 12:20 AM
Joined 4/19/2006
Last visit: 2/25/2014
Posts: 12
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Martin00 wrote:
TomDeWou wrote:

Is there an error message showing somewhere at startup the the cryptographic provider initialization failed? If so, you need to delete the folder C:\Documents and Settings\All Users\Application Data\Microsoft\Crypto - but create a backup before. Then restart your system.


I just had this problem. The solution worked. Thx!

To delete i used the cmd
del /s Crypto
rd /s Crypto



Martin:

There is another folder called Crypto, it´s @ C:\Documents and Settings\Administrator\Application Data\Microsoft\Crypto. At the moment to delete the Crypto folder as the posts said, do this folder remains unchanged?

Can I delete the folder directly from Windows? Because I tried to do it only pressing the delete key, the system only shown that the folder as being deleted, but nothing happened. It remains without change. Or do I have to use the commands you mentioned?

I made a copy of Crypto from the previous posts route, its stored @ my hard disk data partition, in case to need it can I restore it? Or do I need a security backup from Windows directly?

Thank you in advance...
Best regards...
Top
  9/2/2009, 8:38 AM
Joined 11/15/2006
Last visit: 4/24/2014
Posts: 1188
Rating:
Rated: Outstanding [4 out of 5 / rated 125 time(s)]. (125) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

I never heared about anyone who needed the backup, but in such cases I always recommend doing a backup as nobody knows who will be the first one (anyone must be the first blink )


Have Fun!

TomDeWou
Top
  12/31/2010, 8:20 AM
Joined 9/14/2009
Last visit: 3/27/2013
Posts: 19
Rating:
Rated: Outstanding [4 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Some about my solved problem.
I have Field PG M2 with preinstalled software.
In each morning my PG once sporadically rebooted after its power on.
And after this morning reboot ALM lost ALL licenses!!!
Reinstalling is not solved problem.
ALM did not see keys in all drives include floppy drive.
But deleting filder "Crypto" is helping to me.
Thanks.

Top
Thank you for this post from:
12» Page 1 of 2 (11 items)
Actions