Deutsch
Sitemap | Kontakt
Home  |  Products & Solutions  |  News Center  |  e-Commerce  |  Support
Login | Register
[Advanced]
Products
Success stories
Ruggedizing and Refining - SIPLUS extreme
SIPLUS RIC

Success stories: Energy

Container Shell Qatar
SIPLUS RIC at the Munich airport
SMS Messages via Tetra-Funk
Wind Farm interfaced to Control Center to ENERCON GmbH

 Container Shell Qatar
Project: Shell Qatar Container
Location: Qatar
Industrie: Energy
Customer: Siemens PTD M
Project goal: Medium voltage station OPSS4 as container solution

Up to now:

Medium voltage switchgear has been installed in buildings
Delivery of ringle cabinets to the installation site

Solution:

Complete setup of the cabinets in container
Delivery of finished unit to installation site: two container of 18x3 m and one container of 6x3 m, they are placed together as one unit onsite.
Benefits / Achievements:

Savings in the project:
Checked and prewired medium voltage switchgear
Reduced installation and commissioning time
Quicker availability at installation site
Building cost reduced



 SIPLUS RIC at the Munich airport
Project: SIPLUS RIC at the Airport Munich
Location: Munich
Industrie: Energy
Customer: Siemens PTD
Project goal: Telecontrol in medium voltage switchgear

Up to now:

The medium voltage switchgear were installed in buildings with heating
SICAM miniRTU could be used for the telecontrol since no particular environmental conditions were specified

Solution:

The medium voltage switchgear is installed in containers without heating
SIPLUS RIC is specified and thus suitable for use in the container for the extended temperature range
Benefits / Achievements:

Savings in the project:
Extended temperature range
Communications according to IEC 870-5-101 / -104
Compact module with integrated power supply and isolated in-/ outputs



 SMS Messages via Tetra-Funk
Project: Stadtwerke München
Location: München
Industrie: Energy
Customer: Siemens PG
Project goal: Broadcast of SMS Messages via Tetra-Funk

Up to now:

One operator has to be present at the control center to handle the alarms from the Teleperm XP stations
Therefore a second person has to be present (in fact 2 people for 24h a day) to care for the failures on site

Solution:

The automation station Teleperm XP initiates up to 128 SMS messages
SIPLUS RIC S7 broadcasts via TETRA-Funk SMS messages to preselected mobiles
Benefits / Achievements:

Savings in the project:
Messages will be processed in SIMATIC-Manager in form of text-files and can easily be altered.

Savings during operation:
Only one operator necessary, as the SMS messages are broadcast in the whole plant via a mobile to the plant-operator.



 Wind Farm interfaced to Control Center to ENERCON GmbH
Project: Tronder Energi, Norwegen
Location: Wind Farm Valsneset
Industrie: Wind Energy
Customer: ENERCON GmbH
Project goal: Providing Data and Control for local utility

Up to now:

Non-Siemens PLC integrated
No access for the utility to data or control

Solution:

SIPLUS RIC APPLICATION, S7-400 based protocol converter
Standard interface to control unit via IEC 870-5-104
Standard TIA-based communication to control center for future enhancements
Benefits / Achievements:

Savings in the project:
Standard configuration of TIA components
Standard interface according to IEC

Savings during operation:
Reliable communication, no data lost
Easily expandable


Back
Print
   

© Siemens AG 2006-2009 - Corporate Information - Privacy Policy - Terms of Use