Deutsch
Site Map | Contact Us
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support
Login | Register
[Advanced]

Assembling Center SICOMP of Siemens

No-Risk Tailored Automation

Today, complete computer systems should be reliable, cost-effective, and, what is especially important, user-friendly. This is not an easy task, because the demands placed on the complete spectrum of machinery construction are high. However, it is precisely here, that a professional service provider can prove just how valuable he his. A service provider who supplies everything for immediate use. We are such a service provider.



Don´t risk anything - but demand everything!

With our SICOMP Assembling Center, we not only provide thoroughly thought-out complete solutions for your automa-tion tasks, but we also combine existing SICOMP components in accordance with your specific requirements - and that is quite a lot more than you can expect from a normal supplier. Our promoters in your region (refer to the back cover) can help you select the hardware and software components. Then, you only have to give us the appro-priate wiring and setting documentation. We do the rest!


Assembling Center






High Quality - low cost

You can fully depend on us! This is because we draw-up detailed quotations and you benefit in three ways when you order from us:

1. By purchasing a complete system, prices are more favorable than if you were to individually purchase the components on the open market.

2. With our checked and tested systems, you completely exclude any costly risks.

3. You profit by not having to pay for any undesirable delays when installing the system or during the test. Not only this, you have access to the knowhow of our experienced Assembling Center team free-of-charge - which, when it comes down to it, is invaluable...

We place topmost priority on safety

Every system which leaves our facility has been checked down to the finest detail, comes with a complete warranty and is delivered on time. To be absolutely certain, after the system has been connected-up, we carry-out a wiring and run-up test. And - if you require additional tests, then we can arrange this after prior discussion.

Assembling Center




Opinions which count

Wolfgang Koch, VW Wolfsburg, Test System Development:

"Das Assemblingcenter von SICOMP garantiert mir maximale Sicherheit, denn ich erhalte geprüfte Systeme, termingerecht, bei voller Garantieleistung. Und wenn ich mal besondere Anforderungen erfüllen möchte, so bekomme ich das auch!"


Ing. Herbert Wurmb, Elektronik Werkstätte Ing. Wurmb - Sondermaschinenbau, Eichgraben / Austria:

"I am a long-term SICOMP customer and I have been purchasing assembled systems for approximately 3 years now. The openness and modularity of SICOMP systems allows the Assembling Center to integrate my own and third-party components! This means that I get a completely tested system which com-pletely fulfills my requirements."


Michael Hain, Siemens Products and logistics group, Munich

"We receive the completely equipped and tested computer systems ready to power-up - and that, with the highest quality! Simply install the machine, connect the pre-assembled cables and power-up! Even third-party components which we have specified, are integrated into the overall system!"


High-quality service


A completely tested computer system with a full warranty - reliable, fast, favorably priced and exactly as you want it - that is a lot, but it isn't everything that we can do for you. It goes without saying, that we can provide you with every conceivable support and service: We support you across the board, we will provide you with a quotation for your system, and we will deliver on time (also subsequent orders for the computer system which we configured for you) and we are immediately at your side in the unlikely event that your system develops a fault. You can access the support performance of the Assembling Center and the SICOMP Hotline at any time.



Assembling Center












Our Assembling Center can do the following for you:

  • Draw-up a customer-specific system framework
  • Install all of the modules (also components from other product ranges)
  • Set the module adresses
  • Install the software (operating system, driver or applications)
  • Carry out a system- and a function test
  • Full warranty
  • Provide support, Hotline, consultation



... try us out!

Print
   

© Siemens AG 2001-2008 - Corporate Information - Privacy Policy - Terms of Use