Deutsch | Español | Français | Italiano
Site Map | Contact Us
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support
Login | Register
[Advanced]
Publications
Press Center
Events & Trade Shows
Efficiently Controlled
In the Swiss canton of Wallis, the Dutch company DSM Nutritional Products AG has introduced a new concept for saving energy, in which large cooling circuits are equipped with frequency-controlled drives. The new solution not only allows more dynamic control of the plant in comparison with the previous valve control but also offers savings due to the much lower consumption of primary energy.

The Future on the Test Bench
In the immediate neighborhood of the Opel headquarters in Ruesselsheim - in Mainz-Kastel - Opel and GM engineers from GM FCA (General Motors Fuel Cell Activities) have been developing emission-free fuel cell drives since 1998. The ambitious goal: To develop a competitive fuel cell propulsion system by 2010 which is comparable in performance, durability and costs with today's combustion engine powertrains in large quantities. The powertrain modules for the fuel cell automobile from General Motors are being tested on two Siemens test benches since 2004.

Seam Sealing Safe and Sound
DaimlerChrysler AG has developed a new kind of fully automatic application process for body seam sealing in a pilot project. Potential innovations for the company-wide automation standard integraMCG are to be validated and ensured simultaneously for the control-technical implementation of the process.

Print
   

© Siemens AG 2001-2009 - Corporate Information - Privacy Policy - Terms of Use
Full text search
in the NewsCenter