2009-11-19
With the Sinamics DC Master (DCM) the Siemens Drive Technologies Division has expanded its range of drives by a converter for DC applications, thus enabling the Sinamics functions and tools such as SIZER and STARTER to be used.
more
|
2009-11-11
The new Simatic MV420 stationary 1D/2D code reading system from the Siemens Industry Automation Division is characterized by high reading reliability, a compact design, and a wide range of communications and connection options.
more
|
2009-04-16
The range of Industrial Ethernet switches from the Siemens Industry Automation Division has been expanded.
more
|
2009-04-15
The Siemens Industry Automation Division has equipped two new embedded industrial PCs for rough industrial environments with the powerful Intel Core 2 Duo processor.
more
|
2009-03-12
The new Simatic S7-1200 Micro-Controller from the Siemens Industry Automation division is characterized by its versatile and flexible setup concept, along with high performance and an extremely compact design.
more
|
2009-03-06
The new stationary 1D/2D code readers from the Siemens Industry Automation Division are characterized by their high reading reliability and speed as well as by diverse communication and connection possibilities.
more
|
2009-01-27
Siemens“s Industry Automation Division has now redesigned its HF (high frequency) 13.56 megahertz range Simatic RF310R and RF380R RFID (radio frequency identification) read/write devices so that they can also work with ISO 15693 standard transponders (tags).
more
|
2008-11-25
Siemens Drive Technologies is exhibiting the new C240 PN Simotion Controller at the SPS/IPC/Drives Trade Fair. It is a S7-300 format member of the Simotion Motion Control System and has a Profinet interface.
more
|
2008-11-24
Compact block IO modules with Profinet interface are a further addition to the range of distributed IO systems with a high degree of protection (IP65/67) offered by the Siemens Industry Automation Division.
more
|
2008-11-21
The Siemens Industry Automation Division has made the commissioning of Profinet configurations considerably easier.
more
|
previous
|
next
|