English
Sitemap | Kontakt
Home  |  Produkte & Lösungen  |  News Center  |  E-Commerce  |  Support
Login | Registrieren
[Erweitert]
Veröffentlichungen
Presse
Events & Messen

Nuremberg, 16.04.2009

Expanded range of compact Industrial Ethernet switches

The range of Industrial Ethernet switches from the Siemens Industry Automation Division has been expanded. The four new members of the extra-flat Scalance XF-200 product line are ready for use in harsh industrial environments for setting up electrical, optical, or mixed line, star and ring topologies. Also new is the range of Scalance XB-000G switches, which is also being launched with four versions. They are suitable for setting up small Industrial Ethernet star and line topologies in less harsh industrial environments. Expanded range of compact Industrial Ethernet switches
The design of the four new managed switches in the Scalance XF-200 range for setting up electrical, optical, or mixed network structures in an industrial environment corresponds to the design of Simatic ET 200S distributed I/O devices. They can be mounted on a standard mounting rail to save space and are particularly suitable for connecting ET 200S units to Industrial Ethernet/Profinet. There are versions with four and eight electrical RJ45 ports, with six electrical and one optical port, and with four electrical and two optical ports. The inclined cable outlet with retaining collar for the IE FC RJ45 FastConnect connector points downward. This facilitates installation in small control boxes. The new devices can be used in ring structures as redundancy managers and for standby coupling with other network segments to ensure high network availability.
 
The four new unmanaged Scalance XB-000G Industrial Ethernet switches with form factor and compact box form of the Simatic S7-1200 controllers permit space-saving installation in the control cabinet.  They are suitable for setting up small Industrial Ethernet star and line topologies in less harsh industrial environments. There are versions with five and eight electrical RJ45 ports, a version with four RJ45 ports and one multi-mode fiber-optic port, and another version with four RJ45 ports and one single-mode fiber-optic port.
 
Further information can be found on the Internet at: www.siemens.com/scalance
 
Download this press release (pdf):
german english spanish

Download this press release (doc):
german english spanish

A picture accompanies this press release. You can find this picture on the Internet at: www.siemens.com/ad-picture/1910

Informationsnummer: IIA200904.1910e fp

Ansprechpartner: gerhard.stauss@siemens.com

Drucken
   

© Siemens AG 2001-2009  - Impressum - Datenschutz - Nutzungsbedingungen