| Dimension Drawings - Low-Voltage Motors - Siemens | 12/02/2008 10:46 PM | ||
Hide Images |
Print
|

Dimension DrawingsWhen selecting motors, you can obtain an overview about the most important dimensions from the dimension tables provided in Catalog (D81.1):Further,
detailed dimension drawing information is provided in the
Further, we offer 3D Models as step files for various motor types. These files
can be imported and edited in a CAD-System.As soon as a complete Order No. has been entered
or configured with or without codes, a dimension drawing can be called under
the Documentation tab.
These 2D dimension drawings can be displayed and printed
in various views and windows. The appropriate dimension sheets can be exported,
saved and edited/processed as DXF format (Interchange/ Import fomat for CAD systems)
or as bitmap graphics.
However, the number of different models means that
we can only provide the basic types of construction in the SD Configurator.
If you haven’t found the appropriate 3D model, then please send
an e-mail with the Order No. and codes to the following address; we will
make every attempt to respond as quickly as possible to your inquiry:The additional versions
Terminal box positions
Modular mounting concept
2nd shaft end for 1LA9
for frame sizes 063 - 315L can be obtained through the following application: katalog.sd01.aud@siemens.com |