SINAMICS: No. 1 for drive tasks
Drive technology today is characterized by two key trends: On the one hand, the number of variants in mechanical and plant engineering is increasing all the time with the result that drive solutions must be highly flexible and scalable. On the other hand, customers from all sectors of industry demand solutions that are perfectly tailored to their requirements and that are easy to use.
In this context, PROFINET is also being implemented more and more in automation and drive systems. The PROFINET-ready products in the SINAMICS range also move within these circles.
PROFINET in SINAMICS G120 - The modular and reliable converter
PROFINET in SINAMICS G120D - Distributed frequency converter
PROFINET in SINAMICS S120 single-axis device
PROFINET in SINAMICS S120 multi-axis drive group
SIMATIC ET 200S FC and SIMATIC ET 200pro FC