References - SIMATIC NET - Siemens  |   12/02/2008 8:09 PM  
Hide Images  |  Print

SIMATIC NET – References

SIMATIC NET offers solutions that use the advantages of Ethernet and also facilitate the integration of fieldbus systems.
Striking examples include:

In addition to the references accessible via the navigation bar on the left side, there are also references available that were published in technical magazines.


IWLAN with PROFINET and PROFIsafe increases the efficiency of electrolyzer crane systems
To improve the efficiency of the fully automatic electrolyzer crane systems, the Austrian company Hans Kuenz GmbH makes use of wireless communications between central computer, operator panel and safety controller on the crane. The flyer for reference describes the solution implemented.

Teleservice of wind energy plants with MD 740-1 and SCALANCE S612
After the service contracts with the manufacturers expire, many wind energy plants in lower performance classes are upgraded with condition monitoring systems. Especially in smaller plants there are no telephone lines for this purpose and installing them is too expensive and time-consuming. A cost-saving and secure GPRS connection, which has been implemented by Flender Service International, is therefore the suitable solution.

Industrial Wireless Communication >>> New reference flyer
Fully-automated crane control with PROFINET and Industrial WLAN A new reference flyer with the title "Increased productivity and safety: fast and safe loading of steel coils" informs about this application at ArcelorMittal Gent.

SINAUT with SCALANCE S and SCALANCE X
Canal de Isabel II is a public company of the community of Madrid. It supplies, treats and distributes the drinking water to the city. Further, it purifies the waste water.

Telemetry system of water supply is using GPRS / EDGE network
System is based on Siemens GPRS terminals connected with PPI cable to S7-200 controllers

Industrial Wireless LAN instead of wearing cables
The company is part of the Central European group of the British corporation that stands alone in this geographical area supplying customers in the automotive industry, chemical industry, aircraft and space industry as well as machine building from over 50 factories employing 1,800 people.

Measuring data acquisition in the carbon injection system of a blast furnace
Biggest European manufacturer of heavy plates with a top quality product range

Plant-wide process control using PCS7 over Ethernet
AGU Planungsgesellschaft für Automatisierungs-, Gebäude- und Umwelttechnik mbh, Leverkusen, Germany, was founded on April 4,1992 and employs IT specialists, physicists, engineers and technicians.

Rugged Industrial Ethernet network with SCALANCE X switches
The German SiSi plants with headquarters in Heidelberg/Eppelheim have been producing and marketing Capri Sun since 1969 in Germany and Europe.

Rugged Industrial Ethernet network with SCALANCE X switches:
Voith Paper is the process supplier for the international paper industry. Voith Paper develops technical solutions that cover the entire paper production process – from the fiber to the packaged paper.

Reliably producing prefabricated walls. Rugged and secure IWLAN solution
The Carlsberg MUR company employs a highly modern production concept in which brick walls are manufactured fully automatically according to CAD drawings.

Wireless coverage across appx. 4 million square feet of production, office, warehouse and outdoor
Since 1926, The Mt. Olive Pickle Company has grown to be the best selling brand of pickles in the Southeast, and the second-best selling brand of non-refrigerated pickles in the country.

Safety over Wireless in a Gantry Robot:
Implementation for customized & application specific solutions for material handling in the food and printing industry with emphasis on X, Y, Z, Theta machines

Expansion of the system – future oriented, simple and cost-effective:
Complete horizontal and vertical automation for machines and plants, as a part for a part or complete solution

Monitoring of large areas from the control station via a webcam
The agency was formed in 2004. It's tasks include monitoring and securing of industrial/trade facilities and premises.

SINAUT power distribution and wastewater plant:
Engineering company for Electrical engineering, instrumentation and Measurement technology and Quality optimization

Preceding references you will find in the archive.