Motion Control via PROFINET - References - Motion Control Systems - Siemens  |   12/04/2008 5:59 AM  
Hide Images  |  Print
Motion Control via PROFINET

references

GOSS International

PROFINET - superior print quality with reduced maculation

Commercial printing press

In the new concept which has been recently developed for GOSS Sunday machines, 3 to 15 SIMOTION D435/D445 and SINAMICS S120 devices are used depending on the machine size. Up to 50 SINAMICS S120 ranging from 5 to 100 KW as well as 1PH/1FK motors are used as drives. So far, these machines have been equipped with MASTERDRIVES MC. GOSS has already installed the first 4 SIMOTION machines at end customers that successfully use them for manufacturing applications. They have successfully migrated to SIMOTION. Due to this great success, they plan to migrate further GOSS machines to SIMOTION.

All references - Motion Control via PROFINET

Title machine / customer
PROFINET - superior print quality with reduced maculation Commercial printing press
GOSS International
PROFINET ensures ultrafast safe control Retrofitting a press control using PROFINET
IWU Chemnitz, Germany
SIMOTION / SINAMICS / PROFINET in printing machines Web offset printing machine
MAN Roland; Augsburg (Germany)