DOConCD / User Manual Collection - Solutions for cranes - Siemens  |   12/05/2008 3:36 AM  
Hide Images  |  Print

DOConCD / User Manual Collection


SINUMERIK 840D sl/840Di sl/802D sl and SINAMICS
SINUMERIK 840D/810D/840Di/802SCD and SIMODRIVE

The contents of DOConCD have been revised and re-compiled. The contents have been sub-divided into SINUMERIK powerline and SINUMERIK solution line and each have their own DOConCDs. Both productions are supplied on one DVD in German and in English. When installing the software, it can be selected which DOConCD is to be installed. Either all of the productions are complete installed or selected productions.

Up-to-date edition: 04.2008, The DVDs are ordered from LZE
Order No. (MLFB) German/English Edition: 6FC5398-0AC10-0YA2

A DVD with 4 different DOConCD productions is supplied. The DOConCDs for SINUMERIK solution line and SINUMERIK powerline previously contained in one production have now been sub-divided into two productions. Each DOConCD version has German and English documentation on the DVD. As before, we have compiled the complete SINAMICS documentation in a separate DOConCD.
The contents of the DOConCDs are also available on DOConWEB versions.

The following Order No. (MLFB) is available to simplify ordering the latest DOConCD for SINUMERIK and SIMODRIVE or SINUMERIK and SINAMICS:
Order No. (MLFB) German/English Edition: 6FC5298-0CD00-0YG0

Update service

As before, an update service will be offered for this DOConCD:
The update service is valid for one year from the date that the DOConCD is originally ordered. In order to order the update service, the full version must have been purchased. The update contract will be supplied with the actual DOConCD and all of the new editions will be made available over the year. It is assumed that two editions of DOConCD will be issued during the time period of the update contract. The new Edition of the DOConCD is sent for existing update contracts. This applies for both previous update contracts

Order No. (MLFB) German/English Edition: 6FC5298-0CD00-0YG2
The two previously valid Order Nos. will be replaced with the new Order Nos. (MLFB) from July 2007 onwards. The contracts set-up under the previous Order Nos. will still be supplied.

File Size Date
 TOC_pl_1008_de.pdf click here to save 72 KB 10/28/08 Deutsch
 TOC_pl_1008_en.pdf click here to save 70 KB 10/28/08 Englisch
Overview of the documents contained
 TOC_sl_1008_de.pdf click here to save 67 KB 10/28/08 Deutsch
 TOC_sl_1008_en.pdf click here to save 65 KB 10/28/08 Englisch

User Manual Collection

In addition to unilingual DOConCDs, we are offering a User Manual Collection comprising the complete user documentation available in German, English, French, Italian and Spanish.

The latest User Manual Collection can be ordered with the following order no. (MLFB) from RLZE:
MLFB: 6FC5298-7CA00-0YG4

The User Manual Collection comprises the complete user documentation currently available (User Manuals, Programming Guides, Diagnostics Guides, etc.) in the pdf format describing the
SINUMERIK 840D/840Di/810D
SINUMERIK 840D sl/840Di sl
SINUMERIK 802D/802D sl
SINUMERIK 802S/C systems
in German, English, French, Italian and Spanish.
In addition to these language, the CD contains a “Language extensions“ folder comprising the documents available in further languages. You cannot select the pdf files included via the Navigator using the search mechanisms of the User Manual Collection. They can only be displayed as a pdf file.

File Size Date
 TOC_UMC_0608_de.pdf click here to save 51 KB 6/19/08 Deutsch
 TOC_UMC_0608_en.pdf click here to save 52 KB 6/9/08 Englisch
 TOC_UMC_0608_fr.pdf click here to save 51 KB 6/9/08 Französisch
 TOC_UMC_0608_it.pdf click here to save 49 KB 6/19/08 Italienisch
 TOC_UMC_0608_es.pdf click here to save 52 KB 6/19/08 Spanisch

This CD is intended for machine manufacturers who can thus supply the documentation required in different languages on CD together with the machines. The machine manufacturers can print out once the documents required. They are, however, not allowed to market printed versions of the pdf documents stored on the CD.

Scope of functions and handling of the User Manual Collection:
General information on the installation process is provided under "Installation and Handling". After installing the CD, you can select one language using the same navigator as with the DOConCD and select another language at any time.


SINAMICS

Latest edition: 07.2007, multilingual
Available ex stock, to be ordered from LZE

MLFB: 6SL3097-2CA00-0YG4 (German/English/French/Italian)

The DOConCD for SINAMICS comprises all documents required for the SINAMICS S and G systems in German and English. The contents of the SINAMICS CD have been combined in TOC_xx.pdf .
File Size Date
 TOC_de.pdf click here to save 52 KB 9/21/07 Deutsch
 TOC_en.pdf click here to save 51 KB 9/21/07 Englisch
 TOC_fr.pdf click here to save 48 KB 9/21/07 Französisch
 TOC_it.pdf click here to save 49 KB 9/21/07 Italienisch

SIMOTION

The documentation in German, English, Italian and French is supplied together with the SIMOTION product CD. There is no DOConCD for SIMOTION manuals available.


DOConWEB

All DOConCDs are also available as DOConWEB via the Internet:
http://www.siemens.com/automation/doconweb

Installation and Handling

DOConCD requires the widely established Acrobat Reader program. This is available without requiring a license and is therefore free of charge.

The CD is installed using the File Manager/Explorer and the "setup.exe" file. The User Instructions for the DOConCD can be found in the lower area of the file cd_help.pdf.

After DOConCD has been installed, documents can be called up in two ways:

  • using the menu bar under DOConCD or
  • the new "DOConCD" button

After DoconCD is started, a navigator is opened in Acrobat Reader which navigates you when using DOConCD. In this navigator, a full text search can be made, specific document pages can be called through the contents search and a search can be made through an index. The handling is described in detail in the attached online help which is also called up via the navigator. When making a search using the contents, two different routes are offered: Target group oriented via "total contents" and system-oriented using "Groups". The documents are listed according to user, manufacturer and service in the total contents. Under groups, the documents are allocated to the systems. Users can also set-up their own document group under "Own Groups". Using these specified groups and the groups which have been specifically set-up, for the full text search, the scope of the documents involved can be restricted. For example, specific searches can be made in specific documents. In the default setting, all of the documents are searched.
File Size Date
 cd_help_de.pdf click here to save 371 KB 11/3/05 Deutsch
 cd_help_en.pdf click here to save 378 KB 11/3/05 Englisch

List of all available CD-ROMs:

SINUMERIK 840D/840Di/810D/802D/S/C and SIMODRIVE or SINUMERIK 840Dsl/840Disl/802Dsl and SINAMICS:
6FC5298-5CA00-0AG2 (840D SW5, German Edition)
6FC5298-5CA00-0BG2 (840D SW5, English Edition)

6FC5298-6CA00-0AG3 (840D SW6, German Edition)
6FC5298-6CA00-0BG3 (840D SW6, English Edition)

6FC5298-7CA00-0AG4 (840D SW7, German Edition, 04.2006)
6FC5298-7CA00-0BG4 (840D SW7, English Edition, 04.2006)
6FC5298-7CA00-0RG0 (840D SW7, Chinese Edition)

6FC5398-0AC10-0YA2 (840D/840D sl, German/English Edition, 04.2008)

6FC5298-0CD00-0YG0 (the most current Edition German/English)

6FC5298-0CD00-0YG2 (update, contract, new CD Editions supplied)

6FC5298-6CA00-0YG1 User Manual Collection, 840D/840Di/810D User Documentation in five languages, 06.2006 edition
6FC5298-7CA00-0YG3 User Manual Collection, 840D/840D sl/840Di/840Di sl/810D User Documentation in five languages, 06.2007 edition
6FC5298-7CA00-0YG4 User Manual Collection, 840D/840D sl/840Di/840Di sl/810D/802D/802D sl User Documentation in five languages, 06.2008 edition

SINUMERIK 840C/SIMODRIVE
6FC5198-6CA00-0YG3 (840C, SW 5 + 6, German/English Edition)

SINAMICS
6SL3097-3CA00-0YG4
(SINAMICS S, German/English/French/Italian Edition)


Copyright

The CDs as well as all pdf files included are protected by copyright. No part of this CD may be copied by OEMs or end customers without the express written permission of Siemens AG. Publications can likewise only be marketed with the consent of Siemens AG.

Related topics