| Asset - Maintenance - Siemens | 12/05/2008 3:34 AM | ||
Hide Images |
Print
|

| Benefits of plant-based asset management Plant-based Different tasks, different information requirements From the viewpoint of the machine operator, it is primarily information about the production process itself that is of interest while the job of maintenance is to request information about the state of the production equipment. Different tasks, different information requirements Whether the problem is machine operation or machine maintenance, it is the plant's HMI systems, and therefore mostly SCADA stations, which serve as interface between human and machine or plant. It is these over which the relevant user is supposed to be able to find precisely the information important to his task without being flooded with extraneous information. Within the framework of intelligent maintenance strategies, HMI and SCADA systems play a central role in plant-based asset management.
|