| References - High-Voltage AC-Motors - Siemens | 12/05/2008 0:07 PM | ||
Hide Images |
Print
|
Industry Automation and Drive Technologies Portal. |
In order to again significantly increase the capacity of the West-East Pipeline in China - that extends over 4000 km - the operating company has constructed 10 new gas compressor stations.
|
Siemens has further expanded its range with the integration of Loher GmbH and now offers a complete portfolio of explosion-protected drives: from 0.1 kW to 100 MW, with a speed range up to 15,000 rpm also in the megawatt range, as a standard or customized solution and for all applicable ignition protection types in dust and gas atmospheres.
|
The city of Anshan in the northeastern Chinese province of Liaoning is known for its steel industry. Angang Iron & Steel Co. is China's third-largest steel plant. This plant is currently being modernized, a process that also involves installing a new blast furnace blower.
|
Copper mining in the Chilean Andes means mining under extreme conditions: severe frosts and extremely deep snow in winter, and great temperature and humidity fluctuations all year round.
|
Stena Don, a service and investigation oil rig of the latest kind recently started operations in the North Sea. A dynamic positioning system enables accurate positioning to the meter in conjunction with speed-controlled drives.
|
Beijing is not exactly famous as a health resort. Up until now, heating in the Chinese capital has been with heavily sulfurous lignite. The pollution content in the air was accordingly high.
|
| previous | next |