| Multilingualism - SIMATIC HMI - Siemens | 12/05/2008 0:22 PM | ||
Hide Images |
Print
|
|
|
Multilingualism with WinCC flexible
|
|
|
Multilingualism of Engineering Software |
|
|
Engineering of multilingual projects |
|
|
Multilingualism of the Runtime Application |
The Engineering Software is actually available in the European
languages English, French, Spanish, Italian and German and the Asian
languages Chinese
simplified, Chinese traditional, Korean and
Japanese. The configuration interface can be switched between the
installed languages.

WinCC flexible also
supports you in an optimum way when creating multilingual configurations in
up to 32 languages (16 of which can be switched online, depending on the
target device) for worldwide deployment. Switchable views allow operators to
enter configuration data on a multilingual basis.
You can manage
language-dependent texts and graphics in a central text library that carries
out automatic translation on the basis of the system- and user-specific
dictionaries.
The system dictionary included in delivery can be complemented by
user-specific dictionaries which contain terms used for several times within
a configuration.

You can configure texts and graphics on a language-dependent basis. In
this connection, the project can include up to 16 online languages
(including Asian and Cyrillic texts). You can then switch between these
languages at runtime.
This means that different operators can choose the optimum language setting
for their own needs. And if the supplier of a machine or plant is
responsible for servicing and maintenance abroad, the service personnel can
if necessary switch on-site from an Asian language to English, for example,
if you have configured this feature.