Case studies - Redundant WinCC configuration at paintshop of Volvo Trucks factory - SIMATIC HMI - Siemens  |   12/05/2008 7:37 AM  
Hide Images  |  Print
"Optimum from the prime coat"-
Visualization of Cab painting at Volvo trucks
 
The Volvo factory in Umeå is Volvo’s only production site for truck cabs in Europe. In this factory in Northern Sweden, 250 miles away from the Polar Circle, the cabins for all Volvo models are built and then transported to the assembly works in Gothenburg and Gent.
In the course of a capacity extension of the factory a new painting plant for the prime paintwork of the driver cabs had to be installed. Dürr Paint Systems in Stuttgart received the general contract for this. The plant is considered one of the most modern in the world and meets the strictest environmental regulations regarding solvent emissions.Dürr suggested the Siemens AG to the Volvo Truck Corporation as the supplier for the automation and control technology.
Operator station at Volvo factory Umea
The Swedish auto manufacturer decided, after detailed evaluation, to accept Dürr’s suggestion and had its new painting line equipped with Simatic WinCC as a redundant control system and failsafe Simatic S7-400F controllers.
 


Download of case study approx.. 0.2 MB,published in move up 2/2005