| Internet Command, Control & Communication - SIEMENS SCE - Siemens | 12/02/2008 7:33 AM | ||
Hide Images |
Print
|

|
IC3- Internet Command, Control & Communication for SIMATIC S7 installations ![]() Karlsruhe University of Applied Sciences Project manager: Project concept: ![]()
The IC3 project in the university As part of the students project work, they carry out remote diagnosis, remote maintenance and remote programming of SIMATIC-S7 controllers via the Internet. The integration of automation, multimedia (audio/video technology) and Internet technology permits innovative concepts to be developed, which point the way forward. The project covers
The IC3 project in the industrial environment Remote diagnosis, remote maintenance and remote programming are carried out via the Internet for SIMATIC-S7-300 controllers on CD production facilities belonging to STEAG HamaTech AG. This innovative concept makes significant time and cost savings, particularly because a large proportion of the facilities are installed in South East Asia, and until now it has always been necessary for a maintenance technician to drive to the plant when a malfunction occurs. The project covers
Project structure: ![]() |