ASIMON V3
The ASIMON PC software serves the configuration of the AS-Interface safety monitor.
The current state of the configured logic blocks can be read out on-site via
the software’s online function and monitored in the fully graphical diagnostics
view. Thanks to the green/yellow/red color changes of the function blocks and
connecting lines, the desired status information is provided in an intuitive
manner. This function is particularly advantageous for commissioning and troubleshooting.
The ASIMON V3 software offers numerous user advantages such as the fully graphical
circuit diagram illustration of the safety logics in a clear window structure,
safe coupling of two AS-i networks, filtering of short-term single-channel interruptions
in the sensor circuit, management of user-specific blocks, graphical print-out
of the safety logics, successive teach-in or manual entry of ASIsafe code tables,
freely selectable index assignment for integrated PLC diagnostics, immediate
state signaling of relay outputs to the PLC and many more valuable benefits.
 |