| BMW Wackersdorf - AS-Interface - Siemens | 11/23/2008 11:15 AM | ||
Hide Images |
Print
|
Innovative Conveying and Storage Systemswith AS-Interface at the BMW Supply Center in Wackersdorf, Germany
Modular conveying concept with distributed electronic motor starters at
the AS Interface From Wackersdorf to all corners of the globe: with its optimized packaging technique, the new BMW supply center dispatches parts to its production centers in the USA and South Africa. The entire pre-packaging area is linked by a package conveying system with approx. 300 drives. An innovative, modular conveying concept has been developed to fulfill the ambitious time schedule.
Fully distributed motor starter concept:
Approx. 400 distributed electronic AS Interface
compact starters were used.
Customer advantages:
The electronic starters with
the highest operating cycles enable dynamic conveying concepts with the shortest
cycle times. Thus, the conveyors only run when necessary. One of the advantages
of this is that it minimizes the transport buffer.
Optimized stockkeeping: The 2 types of electronic starters cover the whole
spectrum of required motor outputs.
Only one power cable required:
the AS Interface compact starter is fed via a 35A power bus; i.e. the motor starters
assigned to a conveyor segment are supplied by a single line – the efficient
35A power bus.
20% reduction of on-site assembly times
Cable integrated in the conveyor belt profile
|