Sydney Water - Industrial Automation and Control - Siemens  |   11/22/2008 3:00 PM  
Hide Images  |  Print

Digesting bio-sludge for Sydney Water

Siemens Water Technologies has been contracted to provide Sydney Water with a 'bio-sludge' digester which will assist in cleaning local waterways.

Sydney Water

The term 'bio-sludge' is used to classify rubbish and debris captured in metropolitan waterways. As the debris decomposes, methane gas is released which is odorous for local communities and is believed to be one of the causes of global warming.

Siemens Water Technologies Business Development Manager, Rhett Butler, said the Siemens Water Technologies solution, called a Dystor bio-gas holder, is to be installed later in 2006 at North Head in Sydney and will allow Sydney Water to store and digest the bio-sludge in what looks like a futuristic dome.

"The system is an 18-metre diameter cable-restrained membrane of woven design which provides high tensile strength, long fabric life and is resistance to abrasion and ultra-violet rays," said Mr Butler.

"The system also provides an environment for the anaerobic, or oxygen-free, digestion of the bio-sludge as well as storage of the produced methane gas."

The membrane is sealed tight at the digestion tank walls to prevent environmental odours and the entire system can store up to 1,500 cubic metres of methane gas which could potentially be used to generate electricity to heat plant buildings or to run engines which drive pumps and blowers or could be traded on the national electricity market.

The Siemens membrane system has a number of advantages over conventional steel or fibreglass gas holders with floating covers. One advantage is the system can hold up to three times as much gas as conventional systems. Other advantages include reduced maintenance and lower capital and installation costs.

Furthermore, there is no requirement for painting of the membrane or maintaining or replacing the floating cover rollers and slide guides. The flexible membrane also allows much greater travel than rigid cover systems.

Siemens is a preferred automation provider to Sydney Water. In addition to the awarding of the bio-gas holder process technology, Siemens IAC has been selected to provide a totally integrated automation, or TIA, solution for the North Head site.

 "Siemens is pleased to have Sydney Water recognise the benefits of our TIA concept which will involve programmable logic controllers or PLCs, drives and Simocode technology," said Mr Butler.

For more information contact Rhett Butler on +61 2 9491 5415 or by Email.