| Patrick Terminals - Industrial Automation and Control - Siemens | 11/23/2008 6:02 PM | ||
Hide Images |
Print
|
Siemens Crane group recently delivered the electrics for seven twin-lift ship-to-shore post-panamax cranes built by ZPMC of Shanghai, PR China, for Patrick, one of Australia's container terminal operators. The high productivity twin-lift cranes cut an impressive sight on the waterfront of Australia's state capital cities.
The contract involved supply, engineering, manfacture and commissioning of the electrics from the 6.6kV incoming switchgear through to AC drives and motors together with the PLC & SCADA equiipment. A feature of the cranes is the TOUCHMATIC driver enhancement control enabling stress free, automatic positioning of the container from pick-up to put-down points.
Siemens Australia engineers were involved in the project carrying out final commissioning of the cranes at Patrick Terminals located in Brisbane, Sydney, Melbourne and Fremantle.
Siemens Crane group is currently delivering two further crane projects in Australia for Patrick and DPW (formerly P&O Ports) respectively.

Crane type: Ship-To-Shore
OEM: ZPMC, PR China
Year of delivery: 7 cranes 2006
Specifications:
- Hoist: 83/18 T, 75/150 m/min, AC motor 2x 645 kW
- Trolley: 210 m/min, AC motor 4x 75 kW
- Boom: t=5 min, AC motor 220 kW
- Gantry: 50 m/min, AC motors 20x 20 kW
Equipped with:
- AC vector controlled drives with AFE
- SIMATIC S7 automation
- Citect Crane Management System
- Touchmatic-HIPAC semi-automatic positioning system
Location:
- 2x East Swanson Dock - Melbourne
- 2x Port Botany - Sydney
- 2x Fisherman Islands Terminal - Brisbane
- 1x Fremantle
Siemens commenced operations in Australia in 1872 and is now one of this country's most reliable and trusted brands. With well-established businesses in both Australia and New Zealand, Siemens is a diversified technology based solutions provider specialising in power, communications, transportation, healthcare, buildings and automation. At the end of fiscal 2006 (September 2006), Siemens achieved AUD 2.157 billion in sales with 3,460 employees. Siemens in Australia and New Zealand is part of the Siemens global network of innovation which operates in 190 countries throughout the world.