| Post-Panamax - Industrial Automation and Control - Siemens | 11/23/2008 6:04 PM | ||
Hide Images |
Print
|
Siemens Crane group recently delivered the electrics for four twin-lift ship-to-shore post-panamax cranes built by ZPMC of Shanghai, PR China, for DP World (formerly P&O Ports) , one of Australia's container terminal operators. DP World is one of the largest marine terminal operators in the world, with 43 terminals and 13 new developments across 27 countries.
The contract involved supply, engineering, manfacture and commissioning of the electrics from the 11 kV incoming switchgear and transformers through to AC drives and motors together with the PLC & SCADA equiipment. The cranes are the fastest and most powerful to date to be installed in any Australian port.
Siemens Australia engineers were involved in the project carrying out pre-commissioning of the cranes in the manufacturers works in China in addition to the final commissioning of the cranes at DP World terminals located in Brisbane and Melbourne.
Siemens Crane group is currently delivering one further crane project in Australia for Patrick in Port Botany, Sydney .

Crane type: Ship-To-Shore
OEM: ZPMC, PR China
Year of delivery: 4 cranes 200 7
Specifications:
- Hoist: 85/19 T, 90 /180 m/min, AC motor 2x 655 kW
- Trolley: 240 m/min, AC motor 4x 80 kW
- Boom: t=5 min, AC motor 220 kW
- Gantry: 45 m/min, AC motors 20x 18 kW
Equipped with:
- AC vector controlled master drives with 3x parallel AFE
- SIMATIC S7 400 automation
- SICMA Crane Management System with remote CMS PC
Location:
- 2x West Swanson Dock - Melbourne
- 2x Fisherman Islands Terminal - Brisbane
Siemens commenced operations in Australia in 1872 and is now one of this country's most reliable and trusted brands. With well-established businesses in both Australia and New Zealand, Siemens is a diversified technology based solutions provider specialising in power, communications, transportation, healthcare, buildings and automation. At the end of fiscal 2006 (September 2006), Siemens achieved AUD 2.157 billion in sales with 3,460 employees. Siemens in Australia and New Zealand is part of the Siemens global network of innovation which operates in 190 countries throughout the world.