| Bulla Dairy Foods - Industrial Automation and Control - Siemens | 11/23/2008 5:16 PM | ||
Hide Images |
Print
|
|
|
Bulla Dairy FoodsWednesday 6th of August 2004After just 3 months fit out and commissioning, Bulla Dairy Foods in Colac two hours west of Melbourne , began its first production runs. With a reputation as one of the premier manufacturers of liquid dairy product in Australia , the company has now also built an enviable international reputation. Bulla Dairy Foods export to over a dozen countries worldwide. “We have been able to develop these opportunities quickly because we present a quality product. Our clients trust our production methods and depend on our reliability” “Siemens Australia and their partners played a vital role in having us ready to go in April last year. Their ongoing commitment to our plant gives us the confidence we need to ensure our position in these competitive markets”. Andrew Legg, Bulla’s Maintenance Co-Coordinator recalls. “I’ve worked all over the world in the food and beverage industry and I’ve used a number of automation vendors, however when asked for my input in selecting a supplier of an automation solution, I could not go past my experiences with the Siemens product and support” As a part of the Totally Integrated Automation (TIA) strategy, Siemens and it’s partners were able to engineer the Bulla plant from ground up and have it operational in time for April’s first production run. The Siemens approach to automation breaks traditional grounds. Simatic TIA is a tightly integrated software and hardware solution covering project management, programming, total network communications, configuration management and much much more. The Siemens solution at Bulla Dairy Foods is a classical example of Simatic TIA The Colac plant incorporates multiple Siemens S7-200 PLCs, in excess of twenty S7-300 PLCs and one S7-400 PLC with over 7000 I/O points. In addition numerous Siemens HMI panels are installed throughout the plant at machine level. Finally the TIA approach was made complete by implementing an extensive Profibus communications network. Field hardware covering many technologies and numerous vendors are linked into the overall Siemens Automation System enabling complete plant control and monitoring at SCADA level by Siemens WinCC. Because of it’s open architecture based on industry standards the TIA approach permits easy integration of other vendors equipment, thus saving engineering and commissioning time. Andrew Legg adds, “In the context of my experiences, the strength Siemens has always had, lies within its software. Take fault finding for example. Step 7 is extremely flexible in the options it offers within its PLC programming environment. We use the S7 Graph feature, as a form of fault finding by monitoring a number of sequencers across any section of our plant, we track data feed back and evaluate the information as it appears in graph format. We can then target any anomalies in the process”. “Further to that, the Siemens HMI panels we have on site, allow us to import ISO drawings of machine components making identification of problems at component level fast and very easy. We can also import our hardware manuals in the same way”. “We have been completely satisfied with the Siemens outcome. Together with their partners they have provided the complete solution from ground up and their support has been fabulous from day one” “We have a number of plans in place with regards to combining our ERP software with Siemens WinCC. These will mature in the next couple of years. We have no doubt Siemens will again play a vital role in our plans” The Siemens TIA approach at Bulla Dairy Foods in country Victoria represents a complete technology architecture. It has allowed object-orientated software to run the entire family of Automation Systems. |