Deutsch
Contact Us | Site Map
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support
Login | Register
[Advanced]
Products and systems
Vehicle Test Systems
Vehicles and Aggregates
Assembly
Garage
Solutions
Power Train, Research & Development · Engine test rig
Dynamic engine test rig
300 kW three-phase asynchronous generator
In the Porz factory of DEUTZ Motorenwerke AG Cologne, the test stands for diesel engines in the development department were modernized by Siemens Test Engineering Automotive, together with DEUTZ AG.

The test cells were completely renewed and equipped by Siemens with the
following components:

  • Digital test stand controller
  • ET 200S modular test system
  • CATSNT computer-aided test system for recording of measured values and
    automatic control of the test stand

One test stand was equipped for more stringent dynamic requirements by Siemens as follows:

  • Three-phase dynamometer 375 kW/1800 Nm
  • AFE converter with low reaction on system
  • T10FS torque measuring flange

Since we are dealing here with the modernization of test stands already in operation, an exact time schedule must be observed for the conversion of each cell in order to keep the downtime resulting from the conversion as short as possible.

The first modernization phase has been completed and 6 test stands are now in operation. A total of 24 motor test stands are to be modernized up to the same state.

Print
   

© Siemens AG 2001-2008 - Corporate Information - Privacy Policy - Terms of Use